A process that is susceptible for a fire to ignite needs an effective fire suppression system solution.
This section is used for a video description and only a video description. I like kites...
This section is used for a video description. I love Lamp...
Heat treating of steel is essential to the production of durable products. These products are heated in a furnace to the proper temperature and then cooled by some sort of quench: air, salt, special quench fluid, or oil.
Heat treating of metals is essential to the production of durable products. These products are heated in a furnace to the proper temperature and then cooled by some sort of quench medium: air, salt, quench fluid, or oil. The use of oil quenches is wide-spread and the quench facilities generally fall into two categories - open and enclosed. In many Open Quench Tank operations, the parts, as they exit the furnace on the furnace conveyor, drop into an oil bath through a chute. A conveyor, submerged in the oil, carries the parts through the oil for the prescribed time A drip pan under the exit conveyor catches the quench oil draining back into the quench tank. A fume collection hood and exhaust duct create a secondary area for concern.
The process fosters oil vaporization, which can develop into a fire situation easily. Should a fire occur, an automatic CO2 system is discharged onto the burning oil surfaces of the drainboard, hood, exhaust, and oil-coated parts inclusive of the fire hazard. The system can be designed to incorporate the oil tanks, whether they are open or partially enclosed.
See how Kidde Fire Systems products can protect your application. The links below will take you to detailed product information on our fire protection solutions that are recommended for this industry.